Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Secondary PDU's not showing via IP address

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Secondary PDU's not showing via IP address
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
159
Jef
Jef Leader
114
gsterling
gsterling Mentor
77
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
Back to EcoStruxure IT Forum
Start a Topic
jgardner1
jgardner1
Explorer

Posted: ‎2025-05-30 08:44 AM

0 Likes
2
662
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
Posted: ‎2025-05-30 08:44 AM

Secondary PDU's not showing via IP address

The setup we have is the primary PDU has an IP and the secondary PDU is daisy chained, (limited IP Space). On most of the PDU's, the the secondary PDU's show up just fine when logging into the PDU via IP address or DCE. On a handful of them, I cannot get the secondary device to show up. I have tried resetting the module, validated settings on the module, (we are using DHCP set to permanent, not my decision) and checked cabling/ ports between the devices. I tried updating firmware as well with the newest one. What else could it be?

Thank you for any help.

Labels
  • Labels:
  • Data Center Expert
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
VSales
VSales Contributor
Contributor

Posted: ‎2025-06-03 07:08 AM

1 Like
1
622
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
Posted: ‎2025-06-03 07:08 AM

Hello,

 

It is difficult to say what the potential issue is without getting hands-on with the units to understand what is happening. Below are a few potential causes to why the second PDU is not showing up on the NMC.

 

  • If you are having communications problems with Network Port Sharing, check that the total length of network cable between up to four units is not more than 10 meters.
  • If you are having communications problems with Network Port Sharing, check that a terminator (part number 0W04161A or the lower profile version 0W05545A) is installed at both ends of up to four units that can be grouped together.
  • If you are using Network Port Sharing and do not see one or more of the units in the group, check that all units in the group are using the same firmware revision.

If the above doesn't solve your issue, I would highly suggest contacting your local technical support team, they should be able to guide you in the right direction. 

 

Thank You

 

 

Reply

Link copied. Please paste this link to share this article on your social media post.

jgardner1
jgardner1
Explorer

Posted: ‎2025-06-03 12:06 PM

In response to VSales
0 Likes
0
603
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
Posted: ‎2025-06-03 12:06 PM

Firmware could be the issue as it is a couple versions behind. Its weird some work and some don't though. All the cable runs are short 2 meter cables and manufactured (pre-terminated). Thanks for the reply!!!
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.