Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

NBPD0165 direct connection

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • NBPD0165 direct connection
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
fabio.carvalho
fabio.carvalho
Explorer

Posted: ‎2022-09-16 02:20 AM

2 Likes
1
1103
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
Posted: ‎2022-09-16 02:20 AM

NBPD0165 direct connection

Hi Team

 

Is possible to access (see the images) the NBPD0165 camera direct by browser without use the appliance NBRK0750 ?

 

Regards,

 

FC
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
Champion

Posted: ‎2024-05-06 10:35 PM

1 Like
0
890
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
Posted: ‎2024-05-06 10:35 PM

Hi @fabio.carvalho,

 

Yes, it is possible to view a live feed from the camera directly, but it does not directly store clips as that is fully managed by the NetBotz appliance.  If the Camera pod 165 is on the private side of the NetBotz (integration 755 camera, or direct connected to NB via direct ethernet cable), you will need to enable the port forwarding option on the Devices tab and then you can launch into the camera by clicking into the Camera in the devices tab and clicking on the launch icon (3rd blue button).

 

If the camera is on the private network of a NetBotz appliance and was auto discovered and set up the password for it will need to be obtained from the API: https://www.apc.com/us/en/faqs/FAQ000232700/

 

If the device is on your corporates network you should be able to launch directly to it using the button the Camera details view.

 

Regards,

Cory

See Answer In Context

Reply

Link copied. Please paste this link to share this article on your social media post.

Reply 1
Cory_McDonald
Cory_McDonald Champion
Champion

Posted: ‎2024-05-06 10:35 PM

1 Like
0
891
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
Posted: ‎2024-05-06 10:35 PM

Hi @fabio.carvalho,

 

Yes, it is possible to view a live feed from the camera directly, but it does not directly store clips as that is fully managed by the NetBotz appliance.  If the Camera pod 165 is on the private side of the NetBotz (integration 755 camera, or direct connected to NB via direct ethernet cable), you will need to enable the port forwarding option on the Devices tab and then you can launch into the camera by clicking into the Camera in the devices tab and clicking on the launch icon (3rd blue button).

 

If the camera is on the private network of a NetBotz appliance and was auto discovered and set up the password for it will need to be obtained from the API: https://www.apc.com/us/en/faqs/FAQ000232700/

 

If the device is on your corporates network you should be able to launch directly to it using the button the Camera details view.

 

Regards,

Cory
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.