Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

DCE 8.0 - backup size

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • DCE 8.0 - backup size
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Cory_McDonald
Cory_McDonald Champion
159
Jef
Jef Leader
114
gsterling
gsterling Mentor
77
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
Back to EcoStruxure IT Forum
Start a Topic
Jerome_C
Jerome_C
Explorer

Posted: ‎2023-11-28 05:08 AM

1 Like
2
1105
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
Posted: ‎2023-11-28 05:08 AM

DCE 8.0 - backup size

Hi,

For years now, we are using the complete backup option of DCE to store our daily backups on a samba share. It works as expected but since the last update perform early novembre (to 8.0 release), the size of the backup file as been mutiply by 4. It was previously generating a 6 Gb file and now each file is 22 Gb.

I don't remenber if there was a compression option in the 7.x release of DCE, but it looks like the backup file created with the last release is already compressed as a tar.gz command won't have any effect on the size of the file.

Have you already encountered the same issue with the 8.0 release ?

(We are using the 8.0.0.154)

 

Regards,

 

Labels
  • Labels:
  • Data Center Expert
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Replies 2
Gabi
Gabi
Mentor

Posted: ‎2023-12-01 08:54 PM

0 Likes
1
1084
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
Posted: ‎2023-12-01 08:54 PM

Hello,

 

seems like all releases of version 8 have some issues with backup part...beside of removing option to compress backup also minor release 148 have an issue with backup path, release 151 make full backups instead of incremental...so I guess also 154 is not strange regarding backup issues

 

I hope they will release a new version soon in order to fix all this backup issues.....

Like usual, when something is working fine DO NOT TRY to improve it because you will cause another ten issues 🙂

 

Multiple versions of DCE 8.0
The current version of Data Center Expert is 8.0.0.154.
Some customers received DCE 8.0.0.151, DCE 8.0.0.149, or DCE 8.0.0.148.
DCE 8.0.0.154 addresses the following issue in the DCE 8.0.0.151 release:
o Synchronized backups created a Full backup and a new Full backup file.
Synchronized backups now append new data to an existing Synchronized backup as expected.
DCE 8.0.0.151 addresses the following issue in the DCE 8.0.0.149 release:
o Certificates signed by a trusted certificate authority (CA) cannot be removed using the System > Server
Administration Settings > Server Access > Web Server display.
Customers who updated their DCE server to 8.0.0.149 can download the 8.0.0.151 desktop client to
mitigate this issue.
DCE 8.0.0.149 addresses the following issue in the DCE 8.0.0.148 release:
o When the Subdirectory field in the System > Server Administration Settings > Server Backup/Restore
> Backup Share Settings display contains a backslash ( \ ), the backup fails and DCE incorrectly
indicates that the backup was successful.
Replace the backslashes in the Subdirectory field with forward slashes (/) to mitigate this issue

Reply

Link copied. Please paste this link to share this article on your social media post.

Jerome_C
Jerome_C
Explorer

Posted: ‎2023-12-11 01:43 AM

In response to Gabi
0 Likes
0
1060
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
Posted: ‎2023-12-11 01:43 AM

Hi,

After reading some documentation in the help center, i saw that the "compressed" option was available in the back up type of the backup/restore configuration menu. That's the option we used to choose for our backups (not the full as i mentionned above).

https://community.se.com/t5/DCE-server-administration/DCE-server-Backup-Restore/ta-p/446756

Now with the 8.0 release this specific option has been removed from the drop down list (full/synchronized/configuration).

Regards,
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.