Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Creating an Threshold Alarm

EcoStruxure IT Forum

Schneider Electric support forum about installation and configuration for DCIM including EcoStruxure IT Expert, IT Advisor, Data Center Expert, and NetBotz
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
  • Creating an Threshold Alarm
Options
  • Mark Topic as New
  • Mark Topic as Read
  • Float this Topic for Current User
  • Bookmark
  • Subscribe
  • Mute
  • Printer Friendly Page
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
scoop263
scoop263
Explorer

Posted: ‎2021-11-09 08:41 AM

0 Likes
1
1436
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
Posted: ‎2021-11-09 08:41 AM

Creating an Threshold Alarm

I am using Struxureware DCE 7.8.1
I am attempting to create a generic alarm threshold.

This Threshold alarm's purpose is to ensure that any fault that is not a loss of communication will get trigged/ send a short email.
When going through Device alarms for UPS I see "General Fault"

I am unable to find any context to what this Device Alarm entails. Is this device alarm for any issue, or just one that does not fit any of the additional device alarms present in DCE?

If at all possible I would like to find one alarm that could do this instead of utilizing multiple alarms. 

Or is there a way to create a notification policy based off the device, and ignore the Communication Loss alarm - as some of our devices will say that communication was lost for 5 minutes but we already get notified that a site was down, would like to prevent 3 emails for the same exact cause when we already are aware of the issue at hand. 


Labels
  • Labels:
  • Data Center Expert
  • Tags:
  • english
Reply

Link copied. Please paste this link to share this article on your social media post.

  • All forum topics
  • Previous Topic
  • Next Topic
Reply 1
APC_Steve
APC_Steve Leader
Leader

Posted: ‎2021-11-09 09:38 AM

0 Likes
0
1427
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
Posted: ‎2021-11-09 09:38 AM

Hi @scoop263 ,

 

The general fault is indeed a UPS error not covered by another specific device alarm. If you've got a device associated with a specific alarm policy, then you should receive all of the alarms as their levels are configured.

If you create a threshold on an alarm that is already set to send, you will indeed get multiple alarms. 

 

As for threshold alarms, there is really no option that can provide you with a catch-all for UPS alarms. You'd have to set them up individually. 

 

Please also note that any device alarms for an APC device set up with priority scanning should be seen in DCE almost immediately. Device alarms are defined by the device and the device will message DCE when any of them occur. DCE will then poll the device again to verify. If you set up a threshold, you may not see that alarm until the next time the device is scanned.

 

Thanks,

Steve
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.