Connect with IT Design CFD software users to optimize data center equipment layout, cooling, and energy consumption using computational fluid dynamics (CFD).
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Send New InviteClose
Invite a Colleague
Found this content useful? Share it with a Colleague!
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-02-1401:53 PM
Monitor Regions
ITA CFD now supports monitor regions.
Monitor regions are user defined volumes that will report Min/Max/Avg of Temperature, Pressure, and Speed for the volume. The data is available on the tooltip hover over, once an analysis has been run.
A monitor region can be placed just like any other piece of equipment.
They can be adjusted down to the size of a single cell or increased to the size of the entire room.
In the attached screenshot, the monitor region is being used to examine the airflow coming out of the four perforated floor tiles closest to the cooler.
Containment also now reports the same information that the monitor regions do in the hover over tooltip.
If you have questions, send us an email (CFD_support@se.com) or ask here!