Connect with IT Design CFD software users to optimize data center equipment layout, cooling, and energy consumption using computational fluid dynamics (CFD).
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-07-0210:44 AM
Modeling liquid cooled IT racks in ITA CFD
Here are some more details about one of the new features that came out in May, modeling liquid cooled IT racks.
Each IT rack now supports a "Removed by Liquid" option. First, set, the total power for the rack. 40kW? 80kW? 100kW? ITA CFD can handle high power density racks, no problem. Then, set the % of that heat that is removed by liquid.
There are additional "Heat Load" views now, too. In addition to seeing the Total Heat Load, you can view the Heat Load to Air and Heat Load to Liquid, to get a sense of where the heat load is going in your data center. These views will show up automatically in the PDF report as well.