Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2022-06-0804:25 AM. Last Modified: 2022-06-0804:27 AM
Cooling Check Thresholds and more!
Cooling Check Thresholds and more!
Cooling Check Thresholds
The headliner of this update is the Cooling Check thresholds. You can now change the temperature thresholds for IT inlet temperatures as well as thresholds for recirculation. If you only want to focus on IT inlet temperature, you can also disable the recirculation thresholds all together.
This can be found under the Settings menu button in the header. Settings->Cooling Check.
Note that the Cooling Check Thresholds are only available for those with access to the unlimited version of EcoStruxure IT Advisor CFD. (Upgrade to unlimited access here)
Improved Field Value Probing
Highlight Velocity Vector when probing
Probe for values inside Containment
No Leakage construction option for Raised Floor and Dropped Ceiling
Additionally, a bug was fixed with reporting Raised Floor and Dropped Ceiling leakages in the report.