Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84496members
353716posts

Connect to device (M251d)

EcoStruxure Automation Expert / IEC 61499 Forum

Browse this forum to find everything you want to know about EAE and IEC 61499 for distributed control systems. Ask experts your questions, get answers, discuss, and share your experience with the growing community.

Solved
mmoineau
Crewman
Crewman

Connect to device (M251d)

Hello,

 

I would like to connect to my M251d, following the instructions on the documentation with the login installer / *********, but the PLC is always rejecting the connection.

Check the picture below:

Capture_login_M251d.PNG

Is there a way to do a factory reset ?

 

Thank you.

Tags (1)

Accepted Solutions
Santhosh-PB
Crewman Crewman
Crewman
2
1586

Re: Connect to device (M251d)

Hi

 

from the snap the M251d is already configured using another solution and hence the default credentials is no more valid.

if you donot remember the credentials, only way is to reset the device. Please refer to the M251d user manual installed with SW.

Refer to the below chapter on how to use SD Card to reset device.

 

 
 

2022-05-10_16h26_48.png

See Answer In Context

Tags (1)
3 Replies 3
Santhosh-PB
Crewman Crewman
Crewman
2
1587

Re: Connect to device (M251d)

Hi

 

from the snap the M251d is already configured using another solution and hence the default credentials is no more valid.

if you donot remember the credentials, only way is to reset the device. Please refer to the M251d user manual installed with SW.

Refer to the below chapter on how to use SD Card to reset device.

 

 
 

2022-05-10_16h26_48.png

Tags (1)
mmoineau
Crewman
Crewman
0
1555

Re: Connect to device (M251d)

Thank you !

Tags (1)
JacobJ
Crewman
Crewman
0 Likes
0
564

Re: Connect to device (M251d)

Thanks for sharing such a helpful instruction.

Tags (1)