Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).

Esmi Ultima Function Buttons Programming

Building Automation Knowledge Base

Schneider Electric Building Automation Knowledge Base is a self-service resource to answer all your questions about EcoStruxure Building suite, Andover Continuum, Satchwell, TAC…
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
  • Building Automation Knowledge Base
  • Esmi Ultima Function Buttons Programming
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • Intelligent Devices Forum

Previous Next
Contributors
  • Sandeep_Kumar006
    Sandeep_Kumar006

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite
Back to Building Automation Knowledge Base
Start a Topic
Options
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
0 Likes
906 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Esmi Ultima Function Buttons Programming

Sandeep_Kumar006 Troubleshooter
‎2025-02-26 10:19 PM

 

Issue

How to program the function buttons in Esmi Fire Panel

Product Line

ESMI Fire Detection

Environment

  • FFSULH1001.
  • FFSULH1002.
  • FFSULH1003.
  • FFSULH1005.

Cause

Customer wants the specific buttons for specific actions.

Resolution

Up to 24 customer specific, on-screen function buttons may be configured to provide control, disablement and engineering functions.
The function buttons can be configured to be either available or hidden for each log-in profile.
The following procedure describes how to:

  • Set function button attributes/properties.
  • Allocate function buttons to user groups. 
  • Create password specific user accounts for inclusion within a nominated user group.

Setting attributes

Function buttons (inputs) may be set to operate by association to output devices with the same properties e.g. a security input will activate any device that has security ticked as part its output properties, or as part of a cause-and-effect rule where the function button is the “Cause”.

 

  1. With Loop Explorer open, select the Configure menu button and select System Manager to open the function button configuration page.

    Skumar1_0-1740635275941.png

  2. Select the 'Details' button to open the properties section of the function button that you wish to configure.

    Skumar1_1-1740635328412.png

    Note: Input Properties
    The properties page allows the user to configure the input action and associated messages, to set individual colours and either to work as a latched (cleared on user interface reset) or toggled action (press function button to operate and again to turn off). Mapping to zones is optional, and the location text is the name given to the function button when completed.

    Skumar1_2-1740635837455.png

Feature Groups

There are 4 default user groups that can be configured with specific permissions for different users.

 

Skumar1_3-1740635892397.png

 

When configured, the function buttons will be included as selectable options in each of the feature groups. It should be noted that if a function button is allocated to the Logged-out group, then it will be present alongside the User Options button when all other user groups have been logged out. Note that at this level then the user options are limited to system information and basic panel tests such as display colour and LED function.

Sandeep_Kumar006_0-1741582457841.pngSandeep_Kumar006_4-1741582681138.png

Function buttons allocated to User level 2 and 3 may be accessed using the default login codes. If users are to be allocated unique numerical codes, then it would be advisable to change the panel default level 2 and/or 3 codes where required.

Labels (1)
Labels:
  • ESMI Fire Detection
Tags (1)
  • Find more articles tagged with:
  • SandeepKumar25
Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.