Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
View assessments in IT Expert on the Reports > Assessments tab.
Improve inefficiencies through insight into the estimated Level 1 Power Usage Effectiveness (PUE) of your physical infrastructure in the Sustainability assessment.
PUE and DCiE are calculated at the Room level only. Outgoing power from all the UPSs in the room is the indicator of IT load. Metrics are derived from devices and sensor values.
In locations with at least one room and at least one UPS, view the estimated Level 1 PUE and DCiE yearly averages or monthly trends per room over the last 365 days.
PUE
Power Usage Effectiveness (PUE) is the industry-accepted energy efficiency metric for the physical infrastructure systems that support the IT loads of a data center, for example, power and cooling.
PUE is the total facility power divided by the IT load.
DCiE
Data center infrastructure efficiency (DCiE) is a metric used to determine the energy efficiency of a data center, developed by The Green Grid.
It is shown as a percentage, calculated by dividing the IT load by the facility power.
DCiE = IT load / total facility power x 100%
Since exact measurements of utility power are not possible in IT Expert, the Sustainability assessment provides an estimated simple Level 1 PUE and DCiE calculations.
Overview
See the number of rooms in the selected location that have a PUE calculated and are considered Efficient, Average, or Inefficient based on DCiE percentage, limited to 50 rooms per location at this time.
Efficient: DCiE 62.5% or above
Average: DCiE 38.5% - 62.5%
Inefficient: DCiE below 38.5%
Room details
View the PUE, DCiE, Cooling, and detailed energy load information for the past 365 days for each room in locations with at least one room and at least one UPS.
Calculation factors are Power redundancy, Cooling redundancy, and the Cooling medium. The margin of error shown for PUE ( +/- ) is adjusted depending on the information you provide.
You can toggle between yearly PUE values and monthy trends.
Yearly averages
See yearly averages for up to three full calendar years.
Monthly trends
See monthly trends for the last 36 months. You can compare each year to see other trends, such as seasonal temperature changes.
Detailed energy load information
Cooling: The energy used by cooling equipment in the selected room
IT: The energy used by the IT equipment in the selected room. This is used in the PUE calculation.
Power: The energy used by the power equipment in the selected room
Total energy: The total energy load in the selected room
Improve your estimate
Click Improve your estimate to provide information about the calculation factors that influence estimated efficiency:
Power redundancy: 2N, etc.
Cooling redundancy: N1, etc
Cooling medium: Air cooled; Liquid cooled; Chilled water; No cooling; Direct expansion; Not specified
Cooling setup: When available for the selected cooling medium
Selected devices for IT load: Filter to include only the devices you want to include in the calculation.
Note: On the mobile app, you can view the sustainability data only. Log in to IT Expert on a computer to modify configurations to improve the PUE score.
Select devices contributing to IT load
Selecting or deselecting a device impacts the IT load used in PUE calculations.
Select the devices you want to include in the PUE calculation.
All applicable devices in the room are automatically included in the calculation until you specifically deselect them.