Does anyone have a photo of the Glass Touch Panel thermostat showing temperature on the display? Question was asked by interior designer.
Besides the above, I managed to find the information on the following as well - just in case if anyone is also looking for the same, I'm sharing it here:
- Icon size: 10 x 10 mm
- Text Font: Rotobo 8pt
- Display window of the Thermostat is 30 x 12 mm
Thank you!
- Labels:
-
Hotels
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
Hi Anne-Marie,
Unfortunately there aren't many good resources around for the glass panels.
Here is a photo of the rectangular version of the thermostat.
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
Thank you, Richard! Photo is definitely for keeps. A good reference.