Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
Send Wireless SMS Message display
Alert Settings options
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Define the settings for a Send Wireless SMS Message alert action on a NetBotz Appliance configured with a wireless modem.
This alert action is available for a NetBotz Appliance with a modem that supports SMS messaging, installed in or connected to that appliance only.
A name field, severity selections, and the "Alert Action Scheduling" display that all alert action types share,are also available.
Basic tab
Element
Description
Add
Click to add a destination address of the recipients to whom the wireless SMS message alert notification will be sent, in the following format.
sms:sms_device_address
where sms:sms_device_address is the telephone number or e-mail address associated with the SMS-enabled device. For example:
sms:5123334444 or sms:user@mycorp.com
Remove
Click to remove a selected destination from the list.
Include Threshold-specific SMS Destinations
Select to send wireless SMS messages to the destination addresses added to the E-mail tab for NetBotz Appliance alert thresholds.
Note
If the destination addresses list is empty, and Include threshold-specific SMS destinations is not selected, no wireless SMS messages can be sent; if the destination addresses list is empty, and Include threshold-specific SMS destinations is selected, wireless SMS messages can be sent only for thresholds that have an SMS destination address identified in their Threshold-specific address list.
Message
Enter a message for the alert; macros can be used.
Threshold-specific addresses example
A “generic_send_wireless_SMS” alert action is created and no SMS destinations are included.
Include threshold-specific SMS destinations is selected for this "generic_send_wireless_SMS" action.
The “generic_send_wireless_SMS” alert action is added to an alert profile called “alert_profile1.”
The “alert_profile1” profile is specified for two NetBotz Appliance thresholds, “temp_too_high” and “humidity_too_high.”
The “temp_too_high” threshold has Threshold-Specific Addresses for User1 and User2, and the “humidity_too_high” threshold has Threshold-Specific Addresses for User3 and User4.
When “temp_too_high” triggers, only User1 and User2 will receive SMS messages.
When “humidity_too_high” triggers, only User3 and User4 will receive SMS messages.
Advanced tab
Provides elements that further define what a wireless SMS message can include, as well as an Alert Action Scheduling button that allows you to select when an alert action is enabled (all time periods are enabled, by default).
Element
Description
Do Not Send Return-to-Normal Messages
Select if you do not want to send SMS messages when the threshold state returns to normal.
Message Character Size Limit (1 - 160)
Identify the number of characters that can be used in the messages.
Message Validity Period
Select how long a period of time the messages will be valid, from 5 Minutes through 3 Days.