Share Your Feedback – Help Us Improve Search on Community!
Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately.
Click here to take the survey
Send Data to FTP Server display
Alert Settings options
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Define the settings for a Send Data to FTP Server alert action on a NetBotz Appliance.
A name field, severity selections, and the "Alert Action Scheduling" display that all alert action types share, are also available.
Primary and Backup tabs
You must define at least the Primary tab elements.
Note
The only difference between the two tabs is that the Backup tab includes backup settings.
Setting
Description
FTP Server Hostname
Identify the hostname or IP address of the FTP server that will receive the data.
User ID
Identify the user identification needed to log on to the FTP server.
Password
Identify the password needed to log on to the FTP server.
Verify Password
Retype the password.
Target Directory
Identify the relative directory path to be used to store the data at the FTP server. This should always be a path relative to the default directory associated with the user ID used to log on to the FTP server.
If the directories on the path do not exist they will be created automatically.
Note
This Target Directory field accepts macros.
Base Filename
Identify the base filename to be used for storing the data at the FTP server. Pictures from alerts will be stored in files with this name, followed by the *.n.jpg file extension, where n is the picture number (1, 2, 3, etc.).
Alert data will be stored in a file with this name, followed by the *.nbalert file extension.
Pictures include in the data will be stored in files with this name, followed by the *.n.jpg file extension, where n is the picture number (1, 2, 3, etc.).
Note
This Base Filename field accepts macros.
Advanced tab
Provides elements that further define what an e-mail can include, as well as an Alert Action Scheduling button that allows you to select when an alert action is enabled (all time periods are enabled, by default).
Setting
Description
Maximum Camera Pictures
Identify the maximum number of pictures that can be included in the data sent to an FTP server.
Include a Graph with the Alert
Select to include graphs with data sent to an FTP server.
Include Related Maps with the Alert
Select to include related maps with data sent to an FTP server.
Include a Sound Clip with the Alert
Select to include related sound clips in the data sent to an FTP server.
Note
Disabled for NetBotz Appliances that have no audio support.
Picture Export Format
Select the format used for pictures sent with the data sent to an FTP server.
Note
The export options will depend on how the NetBotz Appliance is configured.