Video: Alarm threshold policies in IT Expert

Alarms

How to configure alarm thresholds and alarm notification policies, mute and acknowledge alarms, and test email notifications sent from EcoStruxure IT Expert
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
  • EcoStruxure IT Help Center
  • EcoStruxure IT Help Center Categories
  • IT Expert
  • Configuration
  • Alarms
  • Video: Alarm threshold policies in IT Expert
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
Invite a Co-worker
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
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
Related Forums

  • EcoStruxure IT Forum

  • APC UPS Data Center & Enterprise Solutions Forum

Previous Next

Invite a Colleague

Found this content useful? Share it with a Colleague!

Invite a Colleague Invite

EcoStruxure IT Support

Submit a support request for additional assistance with EcoStruxure IT software.

Request Support
Back to Alarms
Start a Topic
Options
  • Mark as New
  • Mark as Read
  • Bookmark
  • Subscribe
  • Email to a Friend
  • Printer Friendly Page
  • Report Inappropriate Content
2 Likes
5923 Views

Link copied. Please paste this link to share this article on your social media post.

Trying to translate this page to your language?
Select your language from the translate dropdown in the upper right. arrow
Translate to: English
  • (Français) French
  • (Deutsche) German
  • (Italiano) Italian
  • (Português) Portuguese
  • (Русский) Russian
  • (Español) Spanish

Video: Alarm threshold policies in IT Expert

Sisko JLehr Sisko
‎2024-10-01 01:45 AM

 

 

 

 

On this page

 

  • Overview
  • 1. Name the threshold policy; select a location
  • 2. Select sensor types
  • 3. Define the target sensors
  • 4. Configure thresholds
  • 5. Configure hysteresis
  • 6. Summary
  • New state sensor: Gateway Comm Status
  • Overriding alarm threshold policy settings

 

Overview

 

You will only receive notifications on alarms when you connect a Gateway and subscribe to IT Expert or you subscribe devices to Asset Advisor.

 

Most devices come with a set of pre-defined default alarms. While thresholds can be defined directly on devices, like those that use APC Network Management Cards (NMC), it's easier to use threshold policies in IT Expert if you're defining alarm thresholds for sensors on multiple devices.

 

In IT Expert, Administrators and Operators with the appropriate permissions can create alarm threshold policies on numeric and state sensors on the Alarms > Threshold policies page.

 

Multiple threshold policies of the same sensor type are grouped in the list by priority.

Use the icon  ITE drag and drop icon.png  to drag and drop the policy in the list to determine which policy takes precedence when device sensors are in multiple policies.

 

ITE configure threshold policy numeric 1a.png

 

To create a threshold policy:

 

Log in to IT Expert and go to Alarms > Threshold policies. Click Create policy.

 

1. Name the threshold policy; select a location

 

When a device is in multiple threshold policies, the policy in the location closest to the device takes priority.

 

ITE configure threshold policy numeric 2.png

 

2. Select sensor types

 

Select the numeric or state sensor type. Click Show all… to see all available numeric or state sensor types.
Note
: To create a threshold for Battery Capacity Remaining, select Percent. 

 

This example is a Temperature threshold policy.

 

ITE configure threshold policy numeric 3.png

 

3. Define the target sensors

 

Select the target sensors and then narrow your selection. 

The list reflects the number of devices, sensors and locations that meet your criteria.

 

Click Configure in each section to specify what you want to include in the policy and then click Next.

 

Target sensors by:

 

- Device type

- Manufacturer

- Model

- Sensor type

- Sensor name

 

Configure device types

ITE configure threshold policy numeric 41.png

 

Configure device models

ITE configure threshold policy numeric 42.png

 

Configure sensor types

ITE configure threshold policy numeric 43.png

 

 

Otherwise, you can toggle Target specific device sensors only to manually select one or more sensors. Use the Search field narrow your selection.

 

ITE configure threshold policy numeric 6a.png

 

 

4. Configure thresholds

 

Configure the high and low threshold values that cause warning and critical alarms for numeric sensors.

 

You can change the values in the fields to visualize the thresholds in the graph. 

Note: The data shown in the graph are an example, not actual data.

 

Numeric sensor threshold

ITE configure threshold policy numeric 5a.png

 

 

5. Configure hysteresis

 

Hysteresis settings reduce chattering from frequently occurring alarms.

Note: The device always triggers its pre-defined default alarms.

 

Number of violations

Specify the number of times a threshold must be violated before an alarm occurs.

To trigger an alarm without delay, set the number of violations to 1.

Configuring a large number of violations reduces the sensitivity of the threshold alarm.

 

Number of samples

Specify the sample size to be evaluated before an alarm clears. Samples are polling cycles, five minutes by default. 

The sample looks back at that number of polling cycles regardless of whether an alarm has occurred.

Configuring a large sample size compared to violations can delay the alarm from clearing.

 

You can change the values in the fields to visualize the hysteresis in the graph. 

Note: The data shown in the graph are an example, not actual data.

 

ITE configure threshold policy numeric 6.png

 

6. Summary

 

View the summary and save the threshold policy.

 

ITE configure threshold policy numeric 7.png

 

New state sensor: Gateway Comm Status

 

The Gateway Comm Status - protocol  sensor is available for every discovered device: SNMP, Modbus, NetBotz, Redfish.

 

Devices monitored by Gateway 1.23 and newer support configuring hysteresis for communication alarms reported by the Gateway Comm Status sensor.

 

Communication alarms are generated after one violation when devices are not included in a policy for the Gateway Comm Status sensor.

 

To quiet communication alarms for your monitored devices, create a policy, choose the Gateway Comm Status sensor, and configure hysteresis as appropriate.

 

Note: To create a policy to trigger an alarm on the Gateway Comm Status - protocol  sensor without delay, set the number of violations to 1.

 

 

State sensor threshold

ITE configure threshold policy state.png

 

Overriding alarm threshold policy settings

 

You can override the settings on a specific sensor that is included in a threshold policy.

Once you alter the settings, threshold policies will no longer apply to the sensor.

If you delete the threshold configuration on that sensor, any threshold policy settings for the sensor will once again apply.

 

To override a threshold policy on a specific sensor:

 

  1. Go to the details page on the device and select Sensors.
  2. Toggles allow you to see policy-based thresholds and the individual thresholds you have previously configured. Make sure Show policy-based thresholds is selected.
  3. Click the arrow to view the threshold policy settings for the sensor.
  4. Adjust the settings and click Set sensor threshold.

 

ITE override threshold policy settings in sensor details 1.png

 

ITE override threshold policy settings in sensor details 2.png

 

To remove the override and reapply threshold policy settings for the sensor, click Delete sensor configuration.

 

ITE delete sensor config in sensor details.png

 

 

 

 

Was this article helpful? Yes No
No ratings
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
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.