New Community Ranking System
Our Community ranking system has recently been updated. You may notice changes in user rankings and receive system messages or notifications. If you have questions about how the new ranking works, please refer to the announcement post for more details (click here).
CODIGO EN LA PANTALLA DE MI UPS
APC UPS Data Center & Enterprise Solutions Forum
Schneider, APC support forum to share knowledge about installation and configuration for Data Center and Business Power UPSs, Accessories, Software, Services.
Search in
Improve your search experience:
Exact phrase→Use quotes " "(e.g., "error 404")
Wildcard→Use * for partial words(e.g., build*, *tion)
AND / OR→Combine keywords(e.g., login AND error, login OR sign‑in)
Keep it short→Use 2–3 relevant words, not full sentences
Filters→Narrow results by section(Knowledge Base, Users, Products)
Send a co-worker an invite to the portal.Just enter their email address and we'll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
Link copied. Please paste this link to share this article on your social media post.
Posted: 2024-04-1106:25 AM
It would be very helpful if you called out what specific APC UPS model you’re speaking about. As this would help all of us provide more accurate information and feedback. 🙂
Regardless, what happens when you disconnect and remove the actual battery cartridge? The unit should continue to indicate a battery fault is present. ☝️
If so, wait a minute and then (insert and reconnect) the battery cartridge. The unit should see the battery and you can follow the LCD instructions to clear the active fault.
As a reminder the batteries are rated for only 3-5 years of service life. That is based on usage, temperature, and environmental factors. If the batteries are in this range the cartridge may need to be replaced.
The system will perform a self test every 7-14 days depending upon the model, your selection, and available features.
This will complete a small load test on the battery and if it’s good it will pass - if it’s bad the test will fail.
A better and more accurate test is to remove AC Power from the wall. If the unit turns off immediately the batteries are dead - replace.
If the system runs for a specific duration compare that runtime with the APC Runtime Chart. This chart will provide you a rough idea of how many minutes / hours the system will run for based on a new cell with a defined load.
If the expected runtime for a 150 watt load is 60 minutes but you only see 5-10 minutes the battery is end of life - replace.
If however you see 30-45 minutes it’s time to set aside finances and schedule to replace the batteries in the future. 👍
Report back the model UPS and the results of removing and reconnecting the battery cartridge. Along with clearing the active fault message via the LCD Menu. 👍