Posted: 2022-03-06 08:39 AM
APC SMT1500RM2U powers off 10 minutes after being powered on
I have an APC SMT1500RM2U uninterruptable power supply that powers off 10 minutes after being powered on even though it is plugged into a live AC outlet and the battery is 50% charged.
Before powering off this UPS also displays a message that the output is off.
I have reset this UPS to the default settings several times but it continues to do this.
This issue began occurring when I shut this UPS off for several months since I wasn't going to use it.
Now when I power it on it does this and will not stay on.
What can I do to fix this issue so this UPS will stay powered on and won't shut off?
Authentication Failed.
- Authentication Ticket Mismatched, failed authentication.
Link copied. Please paste this link to share this article on your social media post.