Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82608members
350250posts

How can Smart Machines and Robotic improve Line Performance?

Solutions for your Business Forum

No matter if your business is in the retail sector, food manufacturing, or healthcare, you'll find resources and a community of experts to discuss with on content tailored to your industry sector. Subscribe today.

Baris_Aytekin
Crewman Crewman
Crewman

How can Smart Machines and Robotic improve Line Performance?

Consumers’ tastes and behaviours are constantly evolving, particularly in the Food and Beverage industry. It is an industry serving a big number of consumers, so this has an impact on the way manufacturers handle their plant from building, to operating and optimizing. It requires skills and experience from the plant managers to drive their assets in a safe condition.

 

Smart Manufacturing combines smart devices, smart machine processes with software, to increase real-time visibility and to drive the performance of flexible Food and Beverage operations. Solutions like our EcoStruxure platform and architecture can help to transform manufacturing operations for improving flexibility and profitability.

 

Smart machines and robotics is key for ´agile manufacturing´ as it enables motion-oriented automation offers and know-how for outstanding line performance. It is a way to leverage the potential of digitization throughout the machine´s life cycle.

First for design and engineering:

  • Smart design: Reduce time-to-market using simulation technologies

  • Smart engineering: Increase quality and efficiency by automating routine tasks

Then commissioning and operation:

  • Smart commissioning:  Easy commissioning through web visualization, mobile devices and augmented operator

  • Smart operation: Seamless integration of machines in a IT infrastructure open standards

But also, maintenance and services:

  • Smart maintenance: Enhance maintenance efficiency with faster information tracking

  • Smart services: Use digital cloud services to track and monitor machines worldwide

 

EcoStruxure™ Machine is a complete automation solution for food and beverage machinery that combines a variety of applications, services, controllers and connected products thus enabling a shorter time to market, better connectivity, more flexibly and efficiency and as well as more security.

 

Among these solutions, EcoStruxure Machine offers a high-performance packaging application.

One of the key technologies is PacDrive 3 for automating complex high-end machines, which are typically in use for high performance packaging processes in the food and beverage industry. PacDrive 3 is a solution for automating complete machines, including logic, motion and even robotics, with a single controller. Basing on the programming approach and the drive concept it allows a modular approach from both software and mechanical aspects. Basing on sercos communication PacDrive 3 synchronizes a large number of axis within short cycle times and is integrating safety function to improve set-up and maintenance operation (allowing to run the machine at low speed in perfect safety conditions).

 

PacDrive 3 provides a lot of benefits such as the reduction of machine footprints, simplified commissioning and maintenance, accelerated change over from one packaging format to a different one, increased performance and effectiveness and improved energy efficiency.

 

Another available solution is EcoStruxure™ Machine Advisor, which is a cloud-based platform for machine builders. It provides three main benefits:

 

Firstly, tracking machines in operation worldwide thanks to a repository service that enables online access to the machine fleet, documentation, and the history of all machines.

Secondly, remotely monitoring and analyzing machine health and performance via cloud services.

Thirdly, Machine Advisor provides a toolkit to facilitate machine maintenance operations helps with fixing potential incident.

 

SE_Machine_OEE_Recop_Rothaus_900x500.jpg

 

EcoStruxureTM Augmented Operator Advisor is an easy-to-use tool for industrial augmented reality applications. The Solution combines contextual and local dynamic information delivering one mobile experience for both the physical environment and virtual objects. It allows reduced downtime by opening electrical cabinet door virtually. Thanks to an immediate access in the field to real-time data, user manuals, instruction, diagrams etc., the right information is in-place and at every time available, what helps to shorten down times and simplify operation. Furthermore, Machine Advisor reduces human errors by helping to locate the right equipment and by guiding operators step-by-step through complete maintenance procedures.

 

Finally, EcoStruxureTM Machine Expert makes intuitive automation a reality. It is a software for developing, configuring, and commissioning the entire machine in a single software environment. This solution helps saving engineering time by applying complete libraries or even a new machine module. Collaborative engineering help to make the engineering processes more efficient. The code analysis function is a tool of Machine Expert to ensure software quality. Additionally, the software allows to automate efficiently the testing of applications and to simplify the machine commissioning using web visualization and webserver’s technology.

 

To better understand the benefits of applying smart machines and robotics solutions, the case of Somic, the leading builder of the most compact and fastest packaging machines in Germany is perfect:

Somic was trying to resolve various challenges in order to reach high-performance machines for packaging small products. It was essential for them to meet market requirements for innovative, high-performing, and reliable smart machines. They were also looking for a compact solution, a modular design and preventive maintenance using augmented reality.

 

Somic chose EcoStruxure Machine as a solution, including Machine controller, servo drives and motors and EcoStruxure Augmented Operator Advisor.

 

_G9A9958_HD 1080p.jpg

 

The solution allowed higher machine output on minimized footprint, best-in-class maintenance but also fast and immediate access in the field to real-time data, manuals & diagrams. The optimization during operations was made continuous, the time to market shortened and the company achieved energy savings of 40% compared to machines on the market.

Somic´s results were highly satisfying – double the required output with just half of the standard footprint!

 

For more information on Smart Machines and robotics, Agile Manufacturing or on the Food and Beverage industry, join the discussion with experts in the dedicated Exchange Forum.