Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84429members
353627posts

EBO alarms containing @(MonitoredObject->NAME) in the alarm message are not converted in SmartConnector

SmartConnector Forum

Discussion of SmartConnector applications for integration of various other building management systems (BMS) into EcoStruxure Building Operation

Solved
mike_meirovitz
Commander
Commander
0 Likes
1
278

EBO alarms containing @(MonitoredObject->NAME) in the alarm message are not converted in SmartConnector

Hi,

 

We have a SmartConnector extension that is receiving alarms (in real-time) from the EBO. We have a problem with EBO alarms that contains the "@(MonitoredObject->NAME)" in the alarm message field. See the attached screen capture.

 

So for example, if the alarm message is: 

@(MonitoredObject->NAME) is in alarm

or the reset message is:

@(MonitoredObject->NAME) has reset

 

The Smart connector receives the text "@@(MonitoredObject->NAME) is in alarm" instead of D-TMP606-01-00 is in alarm".

 

Is there something we can change in our SmartConnector extension code to convert the @(MonitoredObject->NAME) to the same value that is displayed in the EBO watch window - "D-TMP606-01-00 is in alarm" or "D-TMP606-01-00 has reset"?

 

I appreciate a quick response since a customer is waiting for a solution.

 

Mike

 

 

Attachments
Tags (1)

Accepted Solutions
ardak
Commander Commander
Commander
0 Likes
0
271

Re: EBO alarms containing @(MonitoredObject->NAME) in the alarm message are not converted in SmartConnector

Hello,

 

I'm not sure I fully understand. Some assumptions:

 

  • Your alarms are showing "@(MonitoredObject->NAME) is in alarm" and the corresponding reset message for every alarm, for every monitored object?
  • You want "@(MonitoredObject->NAME)" to change to the monitored object name, like "Temperature sensor" or "D-TMP606-01-00" ?

 

In that case, provide the code you are using to activate the alarms,

 

--Armend

See Answer In Context

Tags (1)
1 Reply 1
ardak
Commander Commander
Commander
0 Likes
0
272

Re: EBO alarms containing @(MonitoredObject->NAME) in the alarm message are not converted in SmartConnector

Hello,

 

I'm not sure I fully understand. Some assumptions:

 

  • Your alarms are showing "@(MonitoredObject->NAME) is in alarm" and the corresponding reset message for every alarm, for every monitored object?
  • You want "@(MonitoredObject->NAME)" to change to the monitored object name, like "Temperature sensor" or "D-TMP606-01-00" ?

 

In that case, provide the code you are using to activate the alarms,

 

--Armend

Tags (1)