Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84784members
354230posts

SCADAPack E Workbench and Utilities 8.18.1 now available for download on Exchange Shop

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

MartinChartrand
Captain Captain
Captain
0 Likes
0
347

SCADAPack E Workbench and Utilities 8.18.1 now available for download on Exchange Shop

Hello SCADA & Telemetry Community,


We are announcing that SCADAPack E Workbench and Utilities 8.18.1 is now available for download on Exchange Shop.

 

SCADAPack E Workbench provides an intuitive, flexible environment for developing, debugging and downloading SCADAPack E Smart RTU logic code.

 

New and improved features for 8.18.1 include:

 

  • SCADAPack 334E RTUs will accept a configuration for a SCADAPack 333E, 314E, 313E and 312E RTUs. When read from the RTU, the device type will report SCADAPack 334E which is the type of the actual device. This feature allows configuration files for 333E, 314E, 313E and 312E RTUs to be used with a SCADAPack 334E without modification.
  • Performance of some DNP3 and 60870-5-101/104 operations was improved for large point count systems.


The following Application and Firmware versions are provided in this download package:

 

  • SCADAPack E Configurator application version 8.18.1.3240
  • SCADAPack 3xxE Firmware version 8.18.1.241.
  • SCADAPack 53xE Firmware version 8.18.1.241.
  • SCADAPack 53xE bootloader version 1.40.
  • SCADAPack 3xxE bootloader version is 2.31.

To access this software download, please <click here>.

 

Thank you.

Martin Chartrand