Remote Operations Forum
Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Posted: 2023-02-03 10:11 AM . Last Modified: 2023-02-03 10:18 AM
Remote Operations Release Announcement
Hello Remote Operations Community,
Remote Operations is pleased to announce the release of RemoteConnect 2.7.4 for SCADAPack™ x70 Smart RTUs.
RemoteConnect is a single software tool for users to monitor, configure, program, and commission SCADAPack™ 470, 474, 570, 574, and 575 Smart RTUs. RemoteConnect is used with EcoStruxure™ Control Expert (Unity Pro), an easy-to-use and powerful IEC 61131-3 logic editor, also used by Modicon™ PLCs.
New! RemoteConnect R2.7.4 includes four major enhancements:
• Significantly faster DNP3 file-read/write performance including optimizations in bandwidth constrained networks using data radios
• Improved file-based datalogging feature with an integrated trend viewing tool by adding support for the SCADAPack 470 and 474 MicroSD card
• OBJ_WriteField logic function block can now be used to write object current value fields where an object is not configured as a logic variable
• Realflo 7.11 support included
The software may be downloaded from the Schneider Electric Exchange Shop page <here>.
It is recommended that prior to installing or upgrading your software version, you read the release notes available from the aforementioned Exchange Shop page (Docs and Videos tab).
Further Information
For additional offer information, please contact James Redmond:
James Redmond, CD
Global Offer Manager – Remote Operations
Process Automation, Industry Business
Phone: +1 (613) 806-2295
Email: James.Redmond@se.com
850 Industrial Ave, Unit 6
Ottawa, Ontario K1G 4K2
Canada
Regards,
Martin Chartrand
Create your free account or log in to subscribe to the forum - and gain access to more than 10,000+ support articles along with insights from experts and peers.