Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84865members
354354posts

RemoteConnect™ 2.7.3 for SCADAPack™ x70 Smart RTUs now available for download from Exchange Shop.

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

MartinChartrand
Captain Captain
Captain
0 Likes
0
167

RemoteConnect™ 2.7.3 for SCADAPack™ x70 Smart RTUs now available for download from Exchange Shop.

Hello Remote Operations community members,


We are pleased to announce the release of RemoteConnect 2.7.3 for SCADAPack x70, the flexible configuration and programming application for SCADAPack x70 Smart RTUs, now available for download from Exchange Shop: <click here>

 

RemoteConnect is a Windows-based application based on EcoStruxure™ Control Expert (Unity Pro) software components that can be used in both local and remote configurations.

 

Highlights include:

  • DNP3 Secure Authentication and DNP3 Data Concentrator are now standard features on all SCADAPack
  • 47x and 57x Smart RTUs
  • New file-based datalogging feature with graphical trend viewing tool
  • Support for a MicroSD card on the SCADAPack 470 and 474 Smart RTUs
  • Support for Modbus broadcast
  • Support for IEC 60870-5-104 Information Object Address (IOA)
  • Updated RemoteConnect Extensions library
  • Updated Realflo Flow Computer 7.10
  • Support for the 6103 power supply module


The software download package consists of:

 

  • RemoteConnect and SCADAPack x70 Utilities 2.7.3
  • SCADAPack x70 Extensions Library for RemoteConnect (included in RemoteConnect)
  • EcoStruxure Control Expert 15.1.


Notes:


1) EcoStruxure Control Expert 15.1 (or newer) is now required when using RemoteConnect 2.7.3 (or newer) and is included in this download package for convenience.

 

2) SCADAPack x70 Extensions Library for RemoteConnect is now included in the RemoteConnect download package and no longer needs to be downloaded separately from this Shop page: https://shop.exchange.se.com/en-US/apps/76149/

 

Thank you.

Martin Chartrand