Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84770members
354204posts

Realflo Flow Computer 7.10.2: Now Available for download from Exchange Shop

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

MartinChartrand
Captain Captain
Captain
0 Likes
0
374

Realflo Flow Computer 7.10.2: Now Available for download from Exchange Shop

Hello Remote Operations Community,


We're pleased to announce the release of Realflo Flow Computer 7.10.2 for SCADAPack Smart RTUs, comprised of the following new features, improvements and fixed issues:

 

New Features:

 

  • Logging of M (Meter) Factor and K Factor can be suppressed for AGA-7 and AGA-9 configuration commands. This reduces the number of logged changes when frequent updates are made to the factors

.

Improvements:

 

  • Three permission controls were added to the Device Lock permissions. These permissions are available when locked: Calibration/Forcing, Realflo Accounts, and Run Execution Control.

 

Fixed Issues:

 

  • Realflo could not log into the ADMIN account after using another account. This is corrected.
  • Realflo did not update the stored PIN if the PIN was changed outside the Realflo application and accounts were later read back by Realflo. This is corrected.
  • Status code 30027 (User is not authorized to perform this function) was returned when changing the ADMIN account pass code from an ADMIN level account. This is corrected.


Application and Flow Computer Versions Contained in this Release:

 

  • Realflo application version is 7.10.3367
  • Flow computer version is 7.10.3367 for SCADAPack 32, 300 series, x70, and 4203
    Flow computer version is 7.01.90 for SCADAPack 16-bit controllers
  • The software package is available for download from Exchange Shop <here>

 

Thank you.
Martin Chartrand