Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84631members
353958posts

New Geo SCADA Expert - Basic MQTT Sample Driver is now available on SHOP Exchange.

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

MartinChartrand
Captain Captain
Captain

New Geo SCADA Expert - Basic MQTT Sample Driver is now available on SHOP Exchange.

For users of Geo SCADA Expert (ClearSCADA):

 

New Geo SCADA Expert - Basic MQTT Sample Driver is now available on SHOP Exchange.

 

MQTT-enabled devices and applications can send and receive telemetry messages in any payload format.

 

This driver allows you to modify its code to use your choice of payloads for data values and control messages and is offered as source code which you can build with Visual Studio. It includes the two parts of the driver and an installer, enabling you to build a package to deploy to Geo SCADA Expert servers.

 

Note: This driver differs from the MQTT driver built into the product installer as it allows a developer to build custom payloads.


Please access this driver's SHOP page by clicking here: https://shop.exchange.se.com/en-US/apps/63177

 

Martin