Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84594members
353860posts

[Imported] RealFLO.tfc File

Remote Operations Forum

Collaborate and share knowledge on the extensive range of remote systems and devices, including SCADA radios and RTUs, on the Schneider Electric Exchange Remote Operations (formerly SCADA & Telemetry) forum. From commissioning SCADA integration devices and software, to enhancing existing installations or troubleshooting, connect with a global community of experts and users. Subscribe today.

sbeadle
Janeway Janeway
Janeway
0 Likes
0
277

[Imported] RealFLO.tfc File

>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<<
User: mchartrand, originally posted: 2018-10-17 18:49:13 Id:82
This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum. The original posters' identities have not been included. Schneider Electric is not responsible for the content of these posts.

-------------------------------

**_loriet:
I have noticed that the *.tfc does not hold the complete meter configuration. For example, I transferred just the *.tfc to another computer to print the configuration, when I opened the file it wasn't complete. The sensor configuration was incorrect. When I transferred all files, *.tf* files and then opened the *.tfc the configuration was correct.
Exactly what files constitute the configuration? It used to be just the *.tfc file._**

______________________

swesley:
Hi Lorie,
You also need the TFS file. The TFS file has the non flow computer settings.
You can also create a template file, but in short you need all the files created for that one.