Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the Exchange portal.Just enter their email address and we?ll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<< User: mchartrand, originally posted: 2018-10-17 19:03:19 Id:88 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------------------
**_ebret: Can RealFLO be installed in more than one PC? The CD with RealFLO can be used to have the PC-based application installed on the field laptop as well on the engineer desktop and the maintenance desktop?_**
_____________________________
mchartrand: RealFLO is sold as a single-user product, however, it's not licensed in any hardware or software way, meaning that from a single copy, multiple installations can be made. That being said, we don't mind if it's installed on a backup machine, but would require that multiple copies be purchased for quantities beyond that.