Support forum for Schneider Electric SCADA systems, radios and RTUs. From commissioning integration devices and software, to enhancing existing installations or troubleshooting.
Send a co-worker an invite to the Exchange portal.Just enter their email address and we?ll connect them to register. After joining, they will belong to the same company.
You have entered an invalid email address. Please re-enter the email address.
This co-worker has already been invited to the Exchange portal. Please invite another co-worker.
Please enter email address
Send InviteCancel
Invitation Sent
Your invitation was sent.Thanks for sharing Exchange with your co-worker.
>>Message imported from previous forum - Category:Realflo Electronic Flow Measurement<< User: mchartrand, originally posted: 2018-10-17 18:59:56 Id:87 This is a re-posting from the obsoleted (October 2018) "Schneider Electric Telemetry & SCADA" forum.
-------------------------------
**_AgentLowe: Would really like to see an expansion module that is compatible with your flow meters. I don't think you currently offer one that will do this but here's to hoping I'm wrong. I also thought I saw were you offered the 4203 with a LAN port in place of the serial port/ports. Is this still an option or was it ever?_**
___________________________
mchartrand: Hello, There are two different versions of the the 4203 (DR and DS) with one having a bit more IO than the other, but the 4203 is effectively not physically IO expandable beyond that, meaning that more IO can't be connected directly to the processor. However, the unit's serial port capability means that you could have a SCADAPack close by with it's expandable IO capabilities, and have the 4203 poll the IO data via Modbus. The ethernet option is not integrated into the 4203, but it is on some of the other SCADASense 4000 modules. That being said though, a third-party serial Modbus-to-Modbus/TCP converter could be used. We sell a Lantronix module that does just that. Please contact our sales support department or your local rep for details.
________________________________
AA: One could simply use a SCADAPack100 on one of the RS232/485 ports and address the I/O on it as if it were on the 4203. This would gain you 3 AI and 6DIO. Hope this helps.