Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84454members
353658posts

New Hardware and Firmware for ION9000 and ION7400!

Power Monitoring and Energy Automation NAM

This forum is created for the exchange of information and open dialogue regarding electrical power monitoring and energy automation products and services. Participants will have access to downloadable material as well as chat opportunities with subject matter experts.

Michael_Neas
Ensign Ensign
Ensign
0 Likes
0
1047

New Hardware and Firmware for ION9000 and ION7400!

New firmware can be found at these links:

ION7400

ION9000

 

Schneider Electric ION meter websites:

ION7400

ION9000

 

This section lists the new functionality that is added to your ION9000 or ION7400 meter after you upgrade to v003.001.000.


4-wire RS-485 Option Module
The 4-wire RS-485 Option Module adds support for 4-wire RS-485 serial communications.  


Fiber Ethernet Option Module
The Fiber Ethernet Option Module adds support for Fiber Optic Ethernet communications.  

 

Framework update
A Power Up Alarm was added to the meter framework for WELMEC compliance. This new default alarm produces a medium priority alarm on the meter display to indicate that a meter power cycle occurred.


Nameplate screen update
The meter nameplate screens were updated to display more meter information and to standardize the nameplate screens across the PowerLogic™ metering platform.

Tags (1)