Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84664members
354053posts

LISG settings on adjustable circuit breakers

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

RLQ
Cadet
0 Likes
2
231

LISG settings on adjustable circuit breakers

i understand the purpose of adjustable breakers in applications where tripping coordination is necessary, but if an adjustable breaker feeds directly to a single load is it suitable to leave the breaker in the factory (most sensitive) setting position?  since there are no other breakers to coordinate with, i see no reason to make any adjustments, is that assumption / observation correct?

2 Replies 2
Christian_Bach
Lieutenant Lieutenant
Lieutenant

Re: LISG settings on adjustable circuit breakers

The settings are usually specified by the installation design office. So it is important to understand & pay attention to the settings.

 

Then if the "factory" settings suit the requirements of the installation / load for safety and continuity of service, no problem to leave them as they are.

 

Hope it answers your question.

 

Christian

Tags (1)
RHH-Eltechna
Commander | EcoXpert Master Commander | EcoXpert Master
Commander | EcoXpert Master

Re: LISG settings on adjustable circuit breakers

Hello @RLQ,

 

Not entirely, you also change settings based on whats in front of the breaker.

Like length and type of cable etc.
We used to have Curve direct for this kind of calculations.

 

Curve Direct

It seems though it changed to a cloud based service which the links doesnt go through, maybe something for SE to solve.

Hope this gives you some insight!


Kind regards,

Rick - Eltechna B.V.
signature-RHHH
Tags (1)