Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84674members
354017posts

Cable Selection types

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Husam-89
Cadet
0 Likes
3
377

Cable Selection types

Hello Guys,

 

I'm working in the LV panel building field , When I select the type of cable from the manufacturer cataloges, 

I see many options regarding the types :

 

- In Conduit or Air

-  Free flat or Free Trefoil

 

Which are the more reasonable options for panels ?

 

Thanks

 

Husam

Tags (1)
3 Replies 3
RHH-Eltechna
Commander | EcoXpert Master Commander | EcoXpert Master
Commander | EcoXpert Master

Re: Cable Selection types

Hello @Husam-89 ,

 

I am not our company's buyer.
However I do know that we use 90 degrees cable and that we defaulted our cable to be Halogen free.
As most of our customers/client demand Halogen free cable's and components nowadays, mostly due fire safety regulation and goals.

 

Hopefully this is of any help!




Kind regards,

Rick - Eltechna B.V.
signature-RHHH
Tags (1)
Lindamartin
Crewman
Crewman

Re: Cable Selection types


@Husam-89 wrote: Rebaid Login

Hello Guys,

 

I'm working in the LV panel building field , When I select the type of cable from the manufacturer cataloges, 

I see many options regarding the types :

 

- In Conduit or Air

-  Free flat or Free Trefoil

 

Which are the more reasonable options for panels ?

 

Thanks

 

Husam


Cable size selection is based on three main factors: Current carrying capacity. Voltage regulation. Short circuit rating.

Tags (1)
sesa378359
Schneider Alumni (Retired)
Schneider Alumni (Retired)

Re: Cable Selection types

Hello @Husam-89 ,

 

These arrangement are to determine the derating of the cable.

 

For fair estimate, the cables inside the panels are to be considered as in conduit because of closed surroundings. This shall have large deration in ampacity.

 

Other point such as flat/trefoil does not have huge impact as the length inside the panel is small for the cables. To have accurate estimate this is to be taken based on the routing of cable inside the panel which will mostly be flat spaced.

 

These are applicable for MV cables and not for LV cables.

 

Hope this clarifies your point.

 

Regards,

 

Aravind.

Tags (1)