Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84612members
353911posts

Alternates to SF6 dielectric mediums in decarbonizing electricity

Power Distribution and Digital

Join experts & peers to learn, share and engage about the key trends of electrical distribution around safety, availability, efficiency and connectivity, as well as power standards & regulations. From design to implementation and operation, let’s discuss how digital and software are transforming your business and your day-to-day work.

Nikita_Sydney
Crewman Crewman
Crewman

Alternates to SF6 dielectric mediums in decarbonizing electricity

Reposting from @DavidKruger . An interesting article on alternates to SF6 dielectric mediums. Have an insightful read!

 

Sulfur hexafluoride (SF6) is a man-made fluorinated gas (F-gas) that has been used for decades in both high voltage (HV) and medium voltage (MV) switchgear. The properties of SF6 made it very well suited for electrical current breaking and insulation.

 

The significantly negative characteristic of SF6 is its’ global warming potential. It is 23,500 times stronger than CO2, making it the single strongest greenhouse gas. The gas is estimated to remain in the atmosphere for 3,200 years.

 

As electrical networks grow, SF6 will continue to proliferate. If no action is taken on SF6, its potential CO2 equivalent impact is expected to increase because of network expansion, including new renewables. By 2050, this would represent a 42% increase on the existing banked volume of SF6 in operation in MV switchgear in Europe alone.

aa.png

 

“In recent years, the technological development of SF6-free medium voltage switchgear has made very good progress,” according to a paper published by Oko-Recherche.

 

The transition to an SF6-free future is now taking shape. The technologies, users, and stakeholders are ready. While a spark is certainly required to achieve the tipping point, this may come from the enabling policy actions that are foreseen.

 

 

For any queries, post them in the comments section!

 

Regards,

Nikita Sydney

Tags (1)
1 Reply 1
Sylvain_C
Lieutenant Lieutenant
Lieutenant

Re: Alternates to SF6 dielectric mediums in decarbonizing electricity

Thanks for the sharing!

 

 

Sylvain Cocheteux - Communication Channels Manager
Tags (1)