Welcome to the new Schneider Electric Community

It's your place to connect with experts and peers, get continuous support, and share knowledge.

Close
Important Announcement: WELCOME to the new Schneider Electric Community! Community is now no longer part of Exchange, and is now rebranded under se.com. If you have any bookmarks and links saved, we request you to update them to ensure that you continue accessing our community from this new location. For any issues that you might encounter as part of this change, please reach out to SchneiderCommunity.Support@se.com, and the team will help to get your issues resolved.
Invite a Co-worker
Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
82501members
350090posts

MODICON M221 EcoStruxure TIMER

Modicon PAC Forum

This forum is for all Modicon users to share knowledge and best practices, submit and discuss ideas for product evolutions and innovation, ask questions and provide answers on the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580, Modicon M340, EcoStruxure Control Expert (Unity Pro), EcoStruxure Process Expert, integration with Aveva Software.

Sanzio94
Crewman
Crewman

MODICON M221 EcoStruxure TIMER

Hello everyone, 

 

I am new to Schneider and EcoStruxure. I am now programming a Modicon M221 with the EcoStruxure Basic Software. It's a simple application that requires a timer, and I want to be able to change the PRESET value through an HMI. I was only able to find a TIMER block that allows an input to start the timer, a fixed PRESET value, and an output Q. 
Is it possible to make the PRESET a variable and change that variable through the HMI?

 

Thank you in advance for your time. 

 

 

Tags (5)
2 Replies 2
Bastian_Schmitz
Commander Commander
Commander

Re: MODICON M221 EcoStruxure TIMER

Hello,

You can reach your goal on the follow way.

You can write a variabel (as example %MW0 which is reachable via Modbus) in the instance of the Timer.

If you use %TM*.P you can overwrite the preseted Time value. (* = number of timer)

 

mm2.PNG

 

best regards

Tags (1)
Sanzio94
Crewman
Crewman
0 Likes
0
703

Re: MODICON M221 EcoStruxure TIMER

Thank you, much appreciated. 

Tags (1)