Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84581members
353849posts

M340 M580 X80 firmware files V5.4

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.

AlastairF
Lieutenant Lieutenant
Lieutenant
0 Likes
1
701

M340 M580 X80 firmware files V5.4

This is a more comprehensive package of links (Firmware link spreadsheet V5.2) than the one provided with SESU.

New update as at 2022-04-12

The attached spreadsheet lists collated links to publicly available firmware for M340/ M580/ X80/ Advantys/ Connexium/ Modicon switches.

Updated with:

M340,
M580 dPAC,
BMENOC,
BMENOS,
Connexium TCSEFE,
PAS600

Feedback welcome (broken links, improvements or additions needed).

The new EcoStruxure Automation Device Maintenance (EADM) tool is now available (link in the spreadsheet). At the moment there is no cloud connectivity for firmware updates so the spreadsheet is still a useful source. Follow the instructions in EADM Help to place the FW files into the correct location for EADM to use.

EADM is mandatory for M580 dPAC, BMENUA and BMENOR module FW upgrades.

Attachments
Tags (1)
1 Reply 1
Trinxs1
Lieutenant Lieutenant
Lieutenant
0 Likes
0
332

Re: M340 M580 X80 firmware files V5.4

thanks Alistair

Trinxs
Senior Technical Sales Consultant - PAC
Tags (1)