Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84400members
353588posts

Control Expert FBD for PM5320?

Modicon PAC Forum

A forum for topics related to the scope of Modicon PAC offers and ecosystem along the whole lifecycle: Modicon M580 and 340, EcoStruxure Control Expert, EcoStruxure Process Expert (Unity Pro) and more.


Accepted Solutions
AlastairF
Lieutenant Lieutenant
Lieutenant

Re: Control Expert FBD for PM5320?

Look at the Modicon GPL libraries - Device library.

There are two DFB's available, one for ModBus serial communication and one for Ethernet communication.

The libraries are available via Exchange (Free)

https://shop.exchange.se.com/en-US/apps/44667/general-purpose-library-for-ecostruxure-control-expert

 

See Answer In Context

Attachments
1 Reply 1
AlastairF
Lieutenant Lieutenant
Lieutenant

Re: Control Expert FBD for PM5320?

Look at the Modicon GPL libraries - Device library.

There are two DFB's available, one for ModBus serial communication and one for Ethernet communication.

The libraries are available via Exchange (Free)

https://shop.exchange.se.com/en-US/apps/44667/general-purpose-library-for-ecostruxure-control-expert

 

Attachments