Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84650members
353993posts

energy meter PM710

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Naif-28
Cadet

energy meter PM710

Why is the customer asking for the standard certificate and are there requirements or instructions from the factory regarding this matter? Is there a time to calibrate from time to time?

2 Replies 2
Charles_Murison
Picard Picard
Picard

Re: energy meter PM710

Hello @Naif-28 ,

 

To start, the PM700 series of meters are obsolete. There is limited information available. Why customer might ask for information is less important than what information is available. It could be some internal audit or just that someone is curious.

 

It may be possible to verify a PM700 meter accuracy (no official process) however there is no way to calibrate the meter.

 

Likely the most you will be able to find for the PM700 is the following PDF:
https://www.se.com/ww/library/SCHNEIDER_ELECTRIC/SE_LOCAL/APS/205891_1A1E/INT_PM200_and_PM700_Calibr...

 

Regards,

Charles

L4 Prime for Advanced metering and Utilities
Tags (1)
greg_expoenergy
Lt. Commander
Lt. Commander
0 Likes
0
223

Re: energy meter PM710

The reason is that many clients which use meters for revenue billing require a calibration certificate in case any billing dispute arises.

Where customer billing and revenue are concerned then it is best to request a/the calibration certificate as a condition of purchase. Larger customers normally use their own check meters to compare with the utility meters and where reading discrepancies arise the first port of call is the meter accuracy and calibration certificate.

I might be wrong but the higher-end ION meters do an A/D calibration based on an internal check reference voltage at startup..