Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84646members
353986posts

New Firmware version 3.1.0 for Advanced Meters is now available!

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Solved
Maaz
Ensign Ensign
Ensign

New Firmware version 3.1.0 for Advanced Meters is now available!

We are excited to announce that the new Firmware V3.1.0 for the advanced meters (PM8000, ION9000, and ION7400) is now available on se.com

 

The Firmware has support for the new Fiber-Ethernet and 4 Wire RS-485 communication option modules and some Framework and Nameplate Screens updates, which will expand the functionality and application range of the meters.  

 

Attached are the What's New documents for more details. 

 

The Firmware can be downloaded from the following links:

Attachments
Tags (1)

Accepted Solutions
Charles_Murison
Picard Picard
Picard
0 Likes
0
1167

Re: New Firmware version 3.1.0 for Advanced Meters is now available!

Thank you for sharing.

 

Charles

 

L4 Prime for Advanced metering and Utilities

See Answer In Context

Tags (1)
1 Reply 1
Charles_Murison
Picard Picard
Picard
0 Likes
0
1168

Re: New Firmware version 3.1.0 for Advanced Meters is now available!

Thank you for sharing.

 

Charles

 

L4 Prime for Advanced metering and Utilities
Tags (1)