Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84645members
353980posts

MID and MIR TECs for PM8000 and ION7400 are now available!

Metering & Power Quality

Collaborate with multiple experts and discuss various topics about Power Meters and Power Quality. From design & implementation to troubleshooting and more, get support from experts and share your experiences by subscribing to the Schneider Electric Exchange forum today.

Maaz
Ensign Ensign
Ensign
0 Likes
1
413

MID and MIR TECs for PM8000 and ION7400 are now available!

We are pleased to announce that in support of our full MID compliance of PM8000 and ION7400, we have received the following EU Type Examination Certificates (TECs) from the SGS:

 

1. Updated MID TEC: Recognition for our latest FW V3.1.0 and adaptation of WELEMEC Guide 11.8

 

2. New MIR TEC: Recognition for use in revenue metering applications in the UK (post-Brexit)

 

Here is the summary of the TECs for PM8000 and ION7400, along with the access links: 

 

Meters

Type

File name and link

PM8000

MID

SGS0203 Schneider PM8000 iss 1 NB0598 ecopy.pdf

MIR

SGS0203 UKCA Schneider PM8000 iss 1 ecopy.pdf

CE DoC

ECDPM8000-MID-A6-V1.pdf

ION7400

MID

SGS0340 ION 7400 iss 1 NB0598 ecopy.pdf                         

MIR

SGS0340 UKCA Schneider ION7400 iss 1 ecopy.pdf

New Firmware version 3.1.0 for Advanced Meters is now available!   

PM8000 and ION7400 are now fully MID compliant!

Attachments
Tags (1)
1 Reply 1
Charles_Murison
Picard Picard
Picard

Re: MID and MIR TECs for PM8000 and ION7400 are now available!

Thank you for sharing.

 

Charles

 

L4 Prime for Advanced metering and Utilities
Tags (1)