Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84850members
354311posts

Here's a basic Glossary that could help when using LayoutFAST

LayoutFAST User Group Forum

The LayoutFAST User Group is a place where Specifiers, Contractors, and Panel Builders share their User experience with the tool and ask Schneider Electric experts questions to solve their issues.

Solved
FelixRamos
Lieutenant JG Lieutenant JG
Lieutenant JG
0 Likes
1
630

Here's a basic Glossary that could help when using LayoutFAST

  • 1A/1B: 1 open & 1 closed Auxiliary Contacts
  • 3W: 3 wire
  • 4W: 4 wire
  • =SE=: Schneider Electric
  • AA: Ambient Air
  • AC: Alternating Current
  • ACB: Air Circuit Breaker
  • AFC: Adjustable Frequency Controller
  • AIC: Amps Interrupting Capacity
  • AIR: Amps Interrupting Rating
  • AMS: Alternative Maintenance Setting
  • ANSI: American National Standards Institute
  • ATS: Automatic Transfer System
  • AWG: American Wire Gauge
  • B2B: Back To Back
  • BFI: Blown Fuse Indicator
  • BIL: Basic Insulation Level
  • BMFD: Blown Main Fuse Detector
  • BMOL: Bimetallic Overload
  • BOM: Bill Of Material
  • bridge
  • bridge objective is to implement Global business Processes supported by One Global Core System associated to Business Transformation in order to enable simplification, improve our business growth and achieve our effiiency goals.
  • For more information see the bridge intranet home page.
  • BTU: British Thermal Unit
  • CAD: Computer Aided Design
  • CB: Circuit Breaker
  • CCT: Common Configuration Team - The Common Configuration Team is a cross-functional team that is responsible for the design, creation, and maintenance of the common processes for product configuration.
  • CCW: Counter Clockwise
  • CDS: Control Disconnect Switch
  • CL: Center Line
  • CLM: Current Limiting Module
  • CM: Circuit Monitor
  • CMH: Component Mounting Hardware
  • CMM: Commercial Multi-Metering
  • CPM: Cycles Per Minute
  • CPS: Cycles Per Second
  • CPT: Control Power Transformer
  • CR: Control Relay
  • CS: Control Switch
  • CSA: Canadian Standards Association
  • CSP: Control Station Panel
  • CT: Current Transformer
  • CTC: Current Transformer Compartment
  • CTU: Capacitor Trip Unit
  • CUL: Underwriters Laboratories of Canada
  • DC: Direct Current
  • DE: Double-Ended
  • DP: Double Pole
  • DPDT: Double Pole Double Throw
  • DPST: Double Pole Single Throw
  • EMAC: Electrical Manufactures Association Of America
  • EUSERC: Electric Utility Service Equipment Requirements Committee
  • EWD: Elementary Wiring Diagram
  • FA: Forced Air
  • FC: Front Connected
  • FCAN: Full Capacity Above Normal
  • FCBN: Full Capacity Below Normal
  • FLA: Full Load Amps
  • FLC: Full Load Current
  • FM: Frequency, Modulation
  • FMCS: Fused Molded Case Switch
  • FP: Freezing Point
  • FPM: Feet Per Minute
  • FPS: Feet Per Second
  • FS: Fusible Switch
  • FVNR: Full Voltage Non-Reversing
  • FVR: Full Voltage Reversing
  • GA: Gage Or Gauge
  • GF: Ground Fault
  • GFCI: Ground Fault Circuit Interrupter
  • GFM: Ground Fault Module
  • GFP: Ground Fault Protection System
  • GFR: Ground Fault Relay
  • GMD: Group Mounted Device
  • GP: General Purpose
  • HACR: Heating, Air Conditioning, And Refrigeration
  • HD: High Density
  • HF: High Frequency
  • HOA: Hand-Off-Auto
  • HP: Horsepower
  • HR: Hand Reset
  • HV: High Voltage
  • HVAC: Heating,Ventilation, and Air Conditioning
  • Hz: Hertz
  • I/O: Input / Output
  • ICCB: Insulated Case Circuit Breaker
  • ID: Inside Diameter
  • IEC: International Electrotechnical Commission
  • IEEE: Institute Of Electrical And Electronic Engineers
  • IER: Integrated Equipment Rating (SCCR Is Correct Term)
  • IMD: Individually Mounted Device
  • IPCPT: Internally Protected Control Power Transformer
  • IPM: Interruptions Per Minute
  • IR: Instantaneous Relay
  • ISO: International Standard Organization
  • ITR: Inverse Time Relay
  • JB: Junction Box
  • kA: kilo Amps
  • kCMIL: Thousand Circular Mils
  • Wire Size
  • KI: Key Interlock
  • KO: Knockout
  • kV: kilo Volts
  • kVA: Kilovolt-Ampere
  • kVAH: Kilovolt-Ampere Hour
  • kVAR: Kilovolt-Ampere Reactive
  • L2R: Left to Right
  • LCD: Liquid Crystal Display
  • LED: Light Emitting Diode
  • LF: Low Frequency
  • LH: Left Hand
  • LO: Lock Out
  • LRC: Locked Rotor Current
  • LS: Low Speed
  • LV: Low Voltage
  • LVR: Low Voltage Relay
  • M-G: Main Generator
  • M-M: Main Main
  • M-T-M: Main Tie Main
  • MAOL: Melting Alloy Overload
  • MC: Momentary Contact
  • MCB: Main Circuit Breaker
  • MCC: Motor Control Center
  • MCCB: Molded Case Circuit Breaker
  • MDGF: Modified Differential Ground Fault
  • MLO: Main Lug Only
  • MV: Medium Voltage
  • MVA: Million Volt Amps
  • N/A: Not Applicable
  • N/R: Not Required
  • NC: Normally Closed
  • NEC: National Electric Code
  • NEMA: National Electrical Manufacurer's Association
  • PCD: Product Configurator Development
  • PPO: Preferred Product Offer - The Preferred Product Offer notations have been established to aid in feature selections (when allowed by specification) giving guidance for items preferred to be supplied by Schneider Electric.
  • PW: Part Winding
  • Q2C: Quote To Cash
  • QED: Quality Engineered Development
  • QMB : Quick Make Break
  • QMQB : Quick Make Quick Break
  • R2L: Right to Left
  • RAM: Random Access Memory
  • RC: Remote Control
  • RIM: Restraint Interface Module
  • For Electronic Circuit Breakers
  • RMS: Root Mean Square
  • ROM: Random Operating Memory
  • RP: Rating Plug
  • For Electronic Circuit Breakers
  • RPM: Revolutions Per Minute
  • RPS: Revolutions Per Second
  • RTT: Ring Tongue Terminal
  • RV: Reduced Voltage
  • RVA: Reactive Volt Ampere
  • RVAT: Reduced Voltage Autotransformer
  • RVNR: Reduced Voltage Non Reversing
  • RVR: Reduced Voltage Reversing
  • RVSS: Reduced Voltage Soft Start
  • SCCR: Short Circuit Current Rating
  • SE: Service Entrance
  • SF: Space Factor
  • SFL: Sub Feed Lug
  • SNA: Schneider North America
  • SP: Special Pricing
  • SPD: Surge Protection Device
  • SPDT: Single Pole Double Throw
  • SPST: Single Pole Single Throw
  • SQD: Square D Company
  • SSOR: Solid State Overload Relay
  • SSTL: Stainless Steel
  • ST: Shunt Trip
  • STSW: Static Transfer Switch
  • SUSE: Suitable For Use As Service Equipment
  • TAG: Technical Assistance Group
  • TC: Trip Coil
  • TFL: Through Feed Lugs
  • TM: Thermal Magnetic
  • TRE: Transparent Ready Equipment
  • TU: Trip Unit
  • TVSS: Transient Voltage Surge Suppressor(see SPD)
  • UCT: Utility Compartment
  • UGPS: Underground Pull Section
  • UL: Underwriters Laboratory
  • ULSE: Underwriters Laboratory Service Equipment
  • UR: UL Listing Type - Component Recognized
  • USA: United States
  • UVR: Under Voltage Relay
  • UVT: Under Voltage Trip
  • VA: Volt-ampere
  • VR: Voltage Relay
  • VSD: Variable Speed Drive
  • VT: Voltage Transformer
  • WHM: Watt-hour Meter
Tags (1)

Accepted Solutions
JeffMMiller
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
582

Re: Here's a basic Glossary that could help when using LayoutFAST

Thanks for the helpful information!

See Answer In Context

Tags (1)
1 Reply 1
JeffMMiller
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
583

Re: Here's a basic Glossary that could help when using LayoutFAST

Thanks for the helpful information!

Tags (1)