Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84572members
353845posts

Replacement fast acting fuses ATS48 for type 2 co-ordination

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Maureen
Crewman Crewman
Crewman

Replacement fast acting fuses ATS48 for type 2 co-ordination

Do we have a replacement for the discontinued fast acting fuses?

If no replacement, does it mean that we don't need the fuses for type 2 co-ordination?

1 Reply 1
BJacqz
Lieutenant Lieutenant
Lieutenant
0 Likes
0
122

Re: Replacement fast acting fuses ATS48 for type 2 co-ordination

The type 2 coordination means it is not necessary to replace any internal component of internal Soft Starter in case of huge damage on motor side (meaning short circuit). In such a case of Short circuit, it is tolerated to check the line contactor (could be light welded but shall be open using a screwdriver) and the fast fuse will protect the internal power components of the Soft Starter (Thyristors).

You can see a table giving fast acting fuses necessary on ATS48 for type 2 coordinationCapture_fastactingfuses_ATS48.PNG.

Tags (1)