Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84412members
353601posts

Long distance SFP module for M580 Hot Standby

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

JerryBartlemay
Ensign Ensign
Ensign
0 Likes
1
270

Long distance SFP module for M580 Hot Standby

I have a customer need for a separation of two M580 hot standby CPUs of at least 13 miles (21 km).  Our standard single mode fiber SFP module has a range of 15 km, or 9.3 miles.  Has anyone tested any high power SFP modules for single mode fiber that have a distance rating of 30-40 km?  

 

While SFP modules are built around a standard, that doesn't mean they are all compatible with all hardware, and so need to be tested.

Tags (1)
1 Reply 1
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
0
152

Re: Long distance SFP module for M580 Hot Standby

Hello @AmeliaFaraci , Could you please support on this? Thanks!

 

Rodrigo G. 


Industrial Automation Community manager

Tags (1)