Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84702members
354079posts

Establish ethernet connection between HMIST6500 and M251

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
jhonut
Ensign
Ensign
0 Likes
5
1758

Establish ethernet connection between HMIST6500 and M251

Hello,

 

I'd like to communicate between HMIST6500 panel and TM251MESE PLC. As driver, in EcoStruxureOperator Terminal, I've chosen Schneider Electric-SoMachineNetwork where I set the PLC IP address (192.168.44.10).

HMI_Driver.PNG

 

In Machine Expert Logic Builder I'm using Generic_EtherNet_IP_device (I'm not sure is the right one). I've set panel's IP address (192.168.44.2) but a red triangle is shown. 

ethernet2.PNG

EthernetIp_device.PNG

 

What am I missing? Are there any other settings I should make in order to be able to have communication between devices?

Another question would be how to address a variable in ESOT through ethernet? For example, if I want to set, from HMI, a value for %MW20, how it should be addressed?

Tags (1)

Accepted Solutions
LeTomas
Lieutenant Lieutenant
Lieutenant

Re: Establish ethernet connection between HMIST6500 and M251

Hi @jhonut ,

 

I have made this video of how to connect the M2xx with an HMI in EOTE (EcoStruxure Operator Terminal Expert):

 

https://schneider-electric.box.com/s/j5liqwbdk3yf6jcmeyp55o3unfqgnf8e

 

I believe this is going to help you.

 

Best regards,

 

Leandro

See Answer In Context

Tags (1)
5 Replies 5
LeTomas
Lieutenant Lieutenant
Lieutenant

Re: Establish ethernet connection between HMIST6500 and M251

Hi @jhonut ,

 

I have made this video of how to connect the M2xx with an HMI in EOTE (EcoStruxure Operator Terminal Expert):

 

https://schneider-electric.box.com/s/j5liqwbdk3yf6jcmeyp55o3unfqgnf8e

 

I believe this is going to help you.

 

Best regards,

 

Leandro

Tags (1)
jhonut
Ensign
Ensign
0 Likes
0
1742

Re: Establish ethernet connection between HMIST6500 and M251

@LeTomas , many thanks for your reply! Though I have one question. How can I have access to https://schneider-electric.app.box.com/ ? I think this kind of videos should be accessed by everyone who's using Schneider software tools. Once again, thank you for your time and solution!

 

Have a great day!

Tags (1)
BenJohnny
Cadet
0 Likes
2
1231

Re: Establish ethernet connection between HMIST6500 and M251

Hi Leandro,

 

I am also struggling to get the HMIST6600 to communicate with a TM251MESE. I followed your video which was great regarding tags, however I can only see that you configured the HMI to talk to the PLC via serial. Can you please give an explanation as to how to configure the communication via Ethernet?

 

Thanks, Ben

Tags (1)
LeTomas
Lieutenant Lieutenant
Lieutenant
0 Likes
1
1223

Re: Establish ethernet connection between HMIST6500 and M251

Hi @BenJohnny ,

 

I have checked the video ( https://youtu.be/ZGvNAPbo-Hs ) and the connection was using the ethernet port of the devices.

 

What you need to do is:

 

On the PLC:

1) Set the ip address and nodename.

2) Add the symbol configuration.

3) Select the variables that you want to share with the HMI.

4) Generate the XML file.

5) Download the app to the HMI ( check if you are going to use the security)

 

On the HMI:

1) Set the ip address of the HMI (same network as the PLC)

2) Add the SoMachine/Machine Expert driver

3) Configure the driver as nodename (use the nodename of the PLC).

4) Check the security on the PLC to match the configuration on the HMI.

5) Import the variable the from the XML file.

6) Download the application to the HMI

 

I believe these are the steps to follow, sorry if miss something in the middle. The video has the complete explanation.

 

Best regards,

Tags (1)
SESA_B
Lt. Commander Lt. Commander
Lt. Commander
0 Likes
0
622

Re: Establish ethernet connection between HMIST6500 and M251

HI Team,

 

I have a  trouble with HIM when I power-on HMI, i accepted but HMI not operation. Pls help me. Thanks very much

IMG_1613 (1).jpg

Tags (1)