Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84462members
353665posts

EcoStruxure operator terminal expert animation problem

Industry Automation and Control Forum

This forum is addressing industrial automation design & engineering, operations, asset performance, cyber security and digital transformation for Plants & Machines.

Solved
baterija
Crewman
Crewman

EcoStruxure operator terminal expert animation problem

Hello

 

I am using ecoStruxure operator terminal expert. 

Is it posible to make an animation of object in correlation of variable value. 

 

For example. 

I am having a switch object and i am using it for input for var1 to control motor. Now i want to animate switch color by the value in Var2. Is this posible? I need this for indication if motor is runing in auto or manual mode and if it is standing or error, so at least 4 diferent status. And also i want to change texts for the sam status. 

 

Thanks

Tags (1)

Accepted Solutions
Lukas
Crewman Crewman
Crewman

Re: EcoStruxure operator terminal expert animation problem

2 Replies 2
Lukas
Crewman Crewman
Crewman

Re: EcoStruxure operator terminal expert animation problem

TomDroll
Lt. Commander Lt. Commander
Lt. Commander

Re: EcoStruxure operator terminal expert animation problem

 

 

Hi, you can BIND a  variable for the ON and OFF state, of the switch - Properties dialog ->Shape->Basic then Off or On state Fill (or Border) color pallet. 

 

See attached screen shot.

Tom Droll
Attachments