Share Your Feedback – Help Us Improve Search on Community! Please take a few minutes to participate in our Search Feedback Survey. Your insights will help us deliver the results you need faster and more accurately. Click here to take the survey
Use this portal to submit your innovative ideas to make Geo SCADA Expert and Devices such as SCADAPack, Trio and Realflo of greater value to you and to the SCADA & Telemetry community. Every idea will be individually reviewed by our team for merit and will be marked Under Consideration.
Search in
| User | Likes Count |
|---|---|
| 2 | |
| 2 | |
| 1 | |
| 1 | |
| 1 |
The SCADAPack E-Series Modbus Scanner functionality allowed for Holding Registers and Input Registers to be used to store packed digital bits, and for these to still be exposed as DNP3 Binary Points without requiring any additional logic / custom code. This was a native function of the E-Series Modbus Scanner.
In the x70, this functionality appears to have been lost, and now it is not possible to map digital bits in Input / Holding Registers into DNP3 Binary Points.
There are a large number of Modbus devices that present all of their data in the Holding Registers, and to have to use custom code in the x70 to map these to DNP3 points is very frustrating. Even more so when the E-series RTUs did this without an issue. It seems crazy that a new RTU family (x70) would be so far less functional than the RTU that it is advertised to replace.
In the Modbus Scanners dialog it should be possible to select Modbus Data Type: UINT and to select Object Type: Digital
Link copied. Please paste this link to share this article on your social media post.
Create your free account or log in to subscribe to the board - and gain access to more than 10,000+ support articles along with insights from experts and peers.