Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84613members
353912posts

Siemens PAC3200 Modbus TCP/IP

Field Devices Forum

Collaborate with a community of professionals and find answers and discuss anything related to the Field Devices (Sensors, Thermostats, Valves & Actuators and more)

Solved
jzotter
Cadet
0 Likes
4
1178

Siemens PAC3200 Modbus TCP/IP

Having issues pulling in correct values in EBO. Does anyone have a tutorial on the proper setup for polling a device? I think it might have to do with the Format from Siemens and EBO doesn't match up exactly, ie. Siemens says Unsigned Long or Float, what is the equivalent in EBO?

Tags (1)

Accepted Solutions
DavidChild
Sisko Sisko
Sisko
0 Likes
2
1152

Re: Siemens PAC3200 Modbus TCP/IP

Tags (1)
4 Replies 4
DavidChild
Sisko Sisko
Sisko
0 Likes
0
1157

Re: Siemens PAC3200 Modbus TCP/IP

Hi,

 

There is plenty of information in the webhelp:

https://ecostruxure-building-help.se.com/bms/topics/show.castle?id=6235&locale=en-US&productversion=...

 

Long could probably mean a 32 (2 word) or 64 (4 word)  bit read, but unsigned and float are two different interpretations of the value.

 

Is the Siemans' modbus documentation available and what registers are you wanting to read?

Tags (1)
DavidChild
Sisko Sisko
Sisko
0 Likes
2
1153

Re: Siemens PAC3200 Modbus TCP/IP

Tags (1)
Alfred69
Crewman
Crewman
0 Likes
0
1092

Re: Siemens PAC3200 Modbus TCP/IP

Tags (1)
derotto
Cadet
0 Likes
0
984

Re: Siemens PAC3200 Modbus TCP/IP


@DavidChild wrote:

Hi @jzotter ,

 

This community post may help too:

 

https://community.exchange.se.com/t5/TAC-Vista-Forum/Interface-to-Siemens-Sentron-PAC3200-power-mete...


This worked for me. Thank you!

Tags (1)