Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84442members
353645posts

Frequent user logon-logoff in GEO SCADA

EcoStruxure Geo SCADA Expert Forum

Find out how SCADA systems and networks, like EcoStruxure Geo SCADA Expert, help industrial organizations maintaining efficiency, processing data for smarter decision making with IoT, RTU and PLC devices.

Solved
BGedco2022
Lt. Commander
Lt. Commander
0 Likes
2
381

Frequent user logon-logoff in GEO SCADA

hello all,

 

Our client has a web based app that reads data remotely from GEO CSDA using ODBC and refresh it in 30s intervals.

They noticed in the event journals, the user logged on and off  frequently and at the same moment similar to the figure below

 

logoff.png

 

 

Does that have any connotation to a problem? And does it affect the performance of the system?

 

appreciate any hint

 

All Respect

 


Accepted Solutions
BevanWeiss
Spock
Spock
0 Likes
1
359

Re: Frequent user logon-logoff in GEO SCADA

It does have a performance impact, since the client and the server are both spending time re-establishing the connection (and session) for each connection.

There is also the performance impact of the GeoSCADA server having to stream this logging information to the disk (as well as just creating it).

 

Best approach would be for the service to retain the connection (either by not disposing of it as frequently, or by pooling the connection if it's used for multiple microservices).

 

It appears to be hitting the server far more frequently than once every 30 seconds also.


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..

See Answer In Context

2 Replies 2
BevanWeiss
Spock
Spock
0 Likes
1
360

Re: Frequent user logon-logoff in GEO SCADA

It does have a performance impact, since the client and the server are both spending time re-establishing the connection (and session) for each connection.

There is also the performance impact of the GeoSCADA server having to stream this logging information to the disk (as well as just creating it).

 

Best approach would be for the service to retain the connection (either by not disposing of it as frequently, or by pooling the connection if it's used for multiple microservices).

 

It appears to be hitting the server far more frequently than once every 30 seconds also.


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
BGedco2022
Lt. Commander
Lt. Commander
0 Likes
0
308

Re: Frequent user logon-logoff in GEO SCADA

thanks @BevanWeiss