Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84733members
354158posts

SE.AppCommonProcess - EAE library for any process application across industries

EcoStruxure Automation Expert / IEC 61499 Forum

Browse this forum to find everything you want to know about EAE and IEC 61499 for distributed control systems. Ask experts your questions, get answers, discuss, and share your experience with the growing community.

Solved
Heleno
Ensign Ensign
Ensign

SE.AppCommonProcess - EAE library for any process application across industries

In an effort to improve user experience and increase engineering efficiency, the Application Libraries have been updated in EcoStruxure Automation Expert.  Now there is set of reusable resources with the most common control modules available in a single Common Process Library (SE.AppCommonProcess), which is already available in the V21.1 release. 

 

Additional control modules such as Totalizer, Multiple Analog Input, Variable Speed Motor, Control Valve, PID Controller, Pulse Width Modulator, Split Range, and Analog Selector are now readily.  For a complete list of the control modules you can reference the next release of documentation when V21.2 is released later this year.  We’re excited to get this update to our users and look forward to your feedback on the Library updates.

App1.png

Tags (1)

Accepted Solutions
Pascal_J
Crewman Crewman
Crewman

Re: SE.AppCommonProcess - EAE library for any process application across industries

Hello Mr JYC .

Release of 21.2 is planned for November 2021.

If you are interested to 'test' I could share a beta version (end of plan) by mid Oct.

Pascal

See Answer In Context

Tags (1)
2 Replies 2
DP-JYC
Lieutenant JG
Lieutenant JG

Re: SE.AppCommonProcess - EAE library for any process application across industries

Hi @Heleno,

 

I would love to give feedback on these news blocs, especially PID. 

 

Do you (or someone else) know when v21.2 is planned?

 

Thx 

Tags (1)
Pascal_J
Crewman Crewman
Crewman

Re: SE.AppCommonProcess - EAE library for any process application across industries

Hello Mr JYC .

Release of 21.2 is planned for November 2021.

If you are interested to 'test' I could share a beta version (end of plan) by mid Oct.

Pascal

Tags (1)