Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84752members
354181posts

Micom PSL Logic Block Descriptions

Ask the Community

New users can ask questions related to our Communities, get tips and tricks on posting and commenting in forums, and solving challenges.

Solved
jaidanbracken
Ensign
Ensign
0 Likes
1
1294

Micom PSL Logic Block Descriptions

Good morning,

I'm looking for a resource that can tell me exactly what each of the blocks in the Micom PSL logic do. I've read the manual for the relay and used the help file but the descriptions in these areas are so vague it leaves me with more questions than answers.

 

On this occasion in particular, I would like to know what the `output signal` does. There is one in a logic diagram with the description of `Protection Trip` and a DDB of 768. This is on a Micom P642.

 

It seems strange that a `Protection trip` is called when the protection has only started, not tripped. There are other instances of this same configuration example where alarm switches on a transformer are mapped to another `Protection Trip`, but the switches are only alarms, not trips.

 

Any help to decypher this would be much appreciated. I would prefer to be shown where to find this information rather than just be told what the answer is. Thanks for any help that can be provided.

 

 

psl.png

 


Accepted Solutions
jaidanbracken
Ensign
Ensign
0
1287

Re: Micom PSL Logic Block Descriptions

Solved.

 

We didn't have the "Technical Manual" available for our particular product. Now that we do, the information is available.

See Answer In Context

1 Reply 1
jaidanbracken
Ensign
Ensign
0
1288

Re: Micom PSL Logic Block Descriptions

Solved.

 

We didn't have the "Technical Manual" available for our particular product. Now that we do, the information is available.