Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84862members
354344posts

Select Object Scada Citect 2018

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.

srosado
Crewman
Crewman
0 Likes
3
825

Select Object Scada Citect 2018

Buenas a todos,

 

me ha surgido la duda acerca de la creación de un menú desplegable para una de las pantallas que estoy realizando desde Citect SCADA Studio 2018. ¿Existe algún object/genie/symbol precargado en Citect que pueda usar o por el contrario, debo crear desde cero un desplegable?

 

Si tienen alguna otra posible solución, estaré encantado de leer sus ideas!

 

Muchas gracias de antemano.

3 Replies 3
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
0
697

Re: Select Object Scada Citect 2018

Gracias por su pregunta!

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
prakashxd
Cadet
0 Likes
0
663

Re: Select Object Scada Citect 2018

I am also looking for similar situation..

Juan
Commander
Commander
0 Likes
0
304

Re: Select Object Scada Citect 2018

Hi,

 

You can create your own popup menu using the DspPopupMenu() function.
It's not complicated, see the help.

 

Regards,

Juan

Tags (1)