Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84601members
353871posts

SCADA CITECT NO ACEPTA PNG

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.

Solved
Xavhiii
Crewman
Crewman
0 Likes
3
1696

SCADA CITECT NO ACEPTA PNG

Estimados colegas, saludos cordiales.

 

Tengo problemas con la importacion de archivos PNG, necesito importar archivos sin fondo o crear simbolos con archivos PNG. no me permite importarlos y si los importa, eston estan en blanco y negro o simplemente no se ve nada.

 

Alguien tuvo el mimso inconveniente? espero su ayuda por favor!

 

 

Gracias.


Accepted Solutions
Richard
Lieutenant Lieutenant
Lieutenant
0 Likes
0
1677

Re: SCADA CITECT NO ACEPTA PNG

The easiest way to do this is to import a normal png with a plain white (or single colour) background, then use Swap Colors from the Tools menu to change the background to transparent (the selection with an x through it).

 

I find this is often easier than using a dedicated graphics package to set a transparent background.

See Answer In Context

Attachments
Tags (1)
3 Replies 3
Rodrigo_Garcia
Administrator Administrator
Administrator
0 Likes
0
1680

Re: SCADA CITECT NO ACEPTA PNG

Hello @sesa222731 , Do you know who can support on this?

 

Regards,

 

R.-

Rodrigo G. 


Industrial Automation Community manager

Tags (1)
Richard
Lieutenant Lieutenant
Lieutenant
0 Likes
0
1678

Re: SCADA CITECT NO ACEPTA PNG

The easiest way to do this is to import a normal png with a plain white (or single colour) background, then use Swap Colors from the Tools menu to change the background to transparent (the selection with an x through it).

 

I find this is often easier than using a dedicated graphics package to set a transparent background.

Attachments
Tags (1)
BevanWeiss
Spock
Spock
0 Likes
0
1666

Re: SCADA CITECT NO ACEPTA PNG

@Xavhiii You're likely to hit a wider target audience if you were to write in English (or at least use Google Translate to include an 'English' version).

 

In regards to wanting to have transparent (alpha channel) PNG files, this is not supported under Citect, as per:

https://www.se.com/au/en/faqs/FA27/

 

So you will typically have to do this in other ways.

You could probably try to get your PNG image into the Citect Graphic Builder and modify it from there to add/remove pixels as necessary.

If the background is always a consistent colour, then you could just replace your transparent sections with this colour to emulate transparency.  More difficult if the content behind is dynamic.


Lead Control Systems Engineer for Alliance Automation (VIC).
All opinions are my own and do not represent the opinions or policies of my employer, or of my cat..
Tags (1)