Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84483members
353700posts

Help file on kernel tables on Citect

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.

Solved
BalajiGuru
Crewman Crewman
Crewman
0 Likes
1
2181

Help file on kernel tables on Citect

Can someone provide a help file which provides information for different Kernel tables available on VJC


Accepted Solutions
RobertSanders
Lieutenant Lieutenant
Lieutenant

Re: Help file on kernel tables on Citect

Hi 

 

The following link is to the Citect 2016 Online help for Kernel commands

 

https://www.citect.schneider-electric.com/webhelp/citect800/#Kernel_Commands_Reference.html?Highligh...

 

The main Kernel command for Citect Runtime information is the PageTable, which can be found 

 

https://www.citect.schneider-electric.com/webhelp/citect800/#Page_Table.html

 

Regards

 

Rob

See Answer In Context

1 Reply 1
RobertSanders
Lieutenant Lieutenant
Lieutenant

Re: Help file on kernel tables on Citect

Hi 

 

The following link is to the Citect 2016 Online help for Kernel commands

 

https://www.citect.schneider-electric.com/webhelp/citect800/#Kernel_Commands_Reference.html?Highligh...

 

The main Kernel command for Citect Runtime information is the PageTable, which can be found 

 

https://www.citect.schneider-electric.com/webhelp/citect800/#Page_Table.html

 

Regards

 

Rob