Send a co-worker an invite to the Exchange portal.Just enter their email address and we’ll connect them to register. After joining, they will belong to the same company.
Send Invite Cancel
84702members
354079posts

EcoStruxure Machine SCADA Expert

AVEVA Plant SCADA Forum

A support forum for AVEVA Plant SCADA (formerly Citect SCADA). Share new and exciting product information, connect, learn, and collaborate with the ecosystem of Plant SCADA Users. AVEVA Plant SCADA a reliable, flexible and high-performance Supervisory Control and Data Acquisition software solution for industrial process customers. This forum is to connect, share, learn and collaborate new and exciting product information. Feel free to join and share to your Ecosystem of Plant SCADA Users.

Solved
FENFEO
Crewman
Crewman
1
1284

EcoStruxure Machine SCADA Expert

What technology is 'Real-time Database' built on? Is it a database or a Cache? If it is a Cache, is this an application cache?


Accepted Solutions
RoozeeR
Lt. Commander Lt. Commander
Lt. Commander

Re: EcoStruxure Machine SCADA Expert

 

Probably a bit confusing terminolgy used from my side, but the real-time database is RAM memory of the SCADA system, not a SQL like database. Best to compare this as application cache memory.

So, when the SCADA system is switched off, the real-time data is lost.

The Real-Time data consist or variables/TAGs filled by data coming from the connected PLCs/RTUs.

These TAGs can be used to visualize, detct alarm levels and LOG to a historical database. The historical database (historian) is a file or database on a harddisk/fileserver.

R.Roozee
Sr Solution Architect (SAE Master)

See Answer In Context

1 Reply 1
RoozeeR
Lt. Commander Lt. Commander
Lt. Commander

Re: EcoStruxure Machine SCADA Expert

 

Probably a bit confusing terminolgy used from my side, but the real-time database is RAM memory of the SCADA system, not a SQL like database. Best to compare this as application cache memory.

So, when the SCADA system is switched off, the real-time data is lost.

The Real-Time data consist or variables/TAGs filled by data coming from the connected PLCs/RTUs.

These TAGs can be used to visualize, detct alarm levels and LOG to a historical database. The historical database (historian) is a file or database on a harddisk/fileserver.

R.Roozee
Sr Solution Architect (SAE Master)